Part Number: TUSB321
Other Parts Discussed in Thread: TMUXHS4212
Tool/software:
In my schematic the VBUS_DET of TUSB321 is 910k. The current mode is connected to grounded via 0 ohm resistor. I have inerfaced it TMUXHS4212 to have USB3 on both sides of the type C. But now only USB2.0 is working. The CC pin detection is happening one side its 3.1V and other is around 0.04V. The USB3 channels are properly routed but not able to detect why is that ?
Can share the schematics in private.