This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB212: Regarding the TUSB212 layout guidelines.

Part Number: TUSB212

Tool/software:

Hi AE,

          The spec only the red-boxed part is useful: route 90Ω traces under the device.

          Could you provide more layout guidelines or related information? Thanls!

  • Hi Bruce,

    The DP/DM traces need to stay connected beneath the USB2 redriver, as the USB2 redriver does not carry the signal through the device. The redriver monitors the DP/DM lanes, and injects current into the signal once it sees a successful HS handshake as the signal moves through the DP/DM lanes beneath it.

    As such, it is recommended to maintain the DP/DM lanes beneath the device, making sure the DP/DM pins on the device touch their respective lanes.

    Thanks,

    Ryan 

  • Hi Bruce,

    I am marking this thread as resolved due to inactivity. If you have any questions or need more assistance, feel free to reply here.

    Thanks,

    Ryan