This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83869HM: Dual 1Gbps Media Converter Application

Part Number: DP83869HM

Tool/software:

Hallo TI-Team,

we developed a hardware with two DP83869HM in unmanaged 1Gbps Media Converter Mode as shown in the following figure:

The Prototype works fine if Near & Far End Link Partner support 1Gbps.

However, it does not work if Near & Far End Link Partner support only 100Mbps.

In that second case, link is up but there is no actual data-traffic.

As Customer would like to use both Near & Far End Link Partner Rate capabilities, the question is if desired function

could be implemented in 1Gbps Media Converter mode or if function mode straps need to be changed to 100Mbps Media Converter mode in second case.

Or in other words: Can DP83869HM unmanaged 1Gbps Media Converter Mode be used for 100Mbps mode as well?

Straps are set the following way:

-Functional - Mode: 1000Base-T to 1000Base-X

- Fiber: Auto-Negotiation  

-Copper: Auto-Negotiation 1000/100, Auto MDIX

-Copper: Mirror Disabled

-Link Loss Pass Thru Enabled