Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB3210 - datasheet of 8052 core required

I have 3 queries below:

1. I need a datasheet of the 8052  core in TUSB3210 - containing the details about the  SFR’s, timer registers (TUSB3210 datasheet says it has tow 16-bit timers need to know the addresses), Port registers (P0-P4: need to know whether to configure them either as input/output) and flag register associated with port2 which can generate interrupt, interrupt configuration, Memory layout  along with instruction manual and debugging interfaces.
Basically need to have a complete data sheet of the 8052 core that is used in the TUSB3210.


2. Can the outputs of TUSB3210 gpio ports (P0, P1, P2 and P3) drive 4mA current when driving a logic high level?
    The datasheet seems to suggest that outputs are open drain type, and can only sink current but not source.

3. There is mention of active pullups (100 uA) on P0, P1, P2 and P3. Are these pullups configurable?
    Also, are the pullups applicable when the ports are configured as outputs?


Please let me know ASAP. Thanks.