Part Number: THVD1400
Tool/software:
Please suggest an SPI to UART converter which can act as master for IIM-42653 Gyroscope sensor , which communicates using SPI Protocol and functions as SPI Slave .
looking for an IC which can :
i) Functions as an SPI Master to communicate with IIM-42653 Sensor .
ii) Can operate with an SPI Clock of ( 24MHz) - as per the sensor's specification.
iii) Support the sensor Output data rate (ODR) of 32KHz ( as per the requirement) - Support continuous SPI read throughput of atleast 3.58Mbps.
Additional References : Checked with ICs : XRM20M1280 , SC16IS762IBS but doesn't find master capabilities.