Other Parts Discussed in Thread: TUSB3410
I am evaluating TIUSB3410 and there are some issues regarding this.
1. When I connect TIUSB3410 UART EVM with the PC, the PC detects it as a separate serial port and things are fine till this step. Then I start hyper terminal and try to see if the letters are typed are echoed back on hyper terminal when I short 2nd and 3rd no pin of serial port (thats how serial port is checked). But letters are not echoed and there is no communication.
2. Then I checked the Rx and Tx pins of TIUSB3410 on the board and I found that when Hyper terminal starts communication the voltage level which is at 3 V goes to 0 V and then when I type the letters to see if there are changes in the voltage levels(which are expected to indicate communication) that does not happen. There is absolutely no change in 0 V that I see on the CRO.
Please suggest me how to proceed from here.