Part Number: TSWDC155EVM
Other Parts Discussed in Thread: ADC3683EVM,
Tool/software:
Hi,
Thanks to @Rob Reeder for providing the required FM/SW/User guide; I am now able to capture data from ADC3683EVM using TSWDC155EVM.
The setup comprises of:
a) ADC3683EVM connected to PC using USB cable
b) Internal CLK and DCLK on ADC3683EVM
c) TSWDC155EVM connected to PC using Xilinx DLC10 JTAG cable
d) Software used: msps server (Refer Fig. E1.png & E3.png) and ADC3683EVM (Refer Fig. E2.png) python client for user configuration and data capturing
Though I am able to acquire the data with the above setup; Currently, I am facing the following issues while capturing data:
1) The data capture is too slow. It takes about 30 seconds to get 30k samples (Refer FIG. E2.png). Can I make it faster, may be less than a second? What changes do I need to do?
2) I do not know how to capture triggered event or set threshold to start the capture
3) I could not capture the Triangular pattern data. Only a flat line was obtained.
Kindly advise to resolve the above issues.
Fig. E1
Fig E2
Fig E3
Thanks & regards,
Nishant