Part Number: DS125BR800
Other Parts Discussed in Thread: DS280BR820
Tool/software:
Hi
I am considering using the DS125BR800 IC with an EEPROM.
In the datasheet, when ENSMB is set to float, it reads 'Read External EEPROM (Master SMBUS Mode)'.
However, just below that, it states that when SNSMB is 1 and READ_EN is low, it 'starts the load from the external EEPROM'.

Will setting READ_EN low cause the EEPROM to be read even when ENSMB is 1?
Also, please explain the difference in operation when setting READ_EN low in the case where ENSMB is float versus when it is 1.

Furthermore, regarding TPOR's 'Time in which a device must be operational after power-on reset',
does this refer to the time required to complete the EEPROM read when READ_EN is held low at all times,
or is it the time for the device to power up and complete the preparation for reading the EEPROM?