Part Number: DS90UH926Q-Q1
Tool/software:
Hello TI team
Is there any limit to the accuracy of the 100R resistor between CMLOUTP & CMLOUTN? Is the recommended accuracy 0.5%, 1%, or 5%?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UH926Q-Q1
Tool/software:
Hello TI team
Is there any limit to the accuracy of the 100R resistor between CMLOUTP & CMLOUTN? Is the recommended accuracy 0.5%, 1%, or 5%?

Hello,
There is not an explicit limit for the 100Ω termination. Unless the oscilloscope you plan to use does not have an included 100Ω termination, then the resistor shown in the application diagram is not required. If an external termination is required, the recommended accuracy is 1% at most. The DS90UH926-Q1 EVM uses a 0.5% resistor.
Most oscilloscopes will have internal termination accuracy around 2%-3%
Best,
Jack