This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unused pins on TUSB2046B hub?



If the customer does not need to use all the 4 ports how should they connect the unused pins for the unused ports. Is it necessary to terminate them?

  •  

    The DP and DM signals of the unused port should be tied to ground with 15K resistors like the pull-downs used on the active ports.

    The OVRCUR/ input of the unused port can be left tied to the other OVRCUR/ inputs if the hub is configured as GANGED.

    If the hub is not configured as GANGED, OVRCUR/ input of the unused port should have a pullup resistor.  A value of 1.5K is sufficient.

    The PWRON/ output can be left unconnected.