Other Parts Discussed in Thread: DS34RT5110
I am using the HDMI DS34RT5110 with various CAT 5e and CAT 6 cables (2 of them obviously). I can make the system work for DVD viewing with the following configuration: DVD player -> HDMI cable->DS34RT5110 driver board->two Category cables ->DS34RT5110 Receiver-> HDMI cable ->TV
When I test the HDMI receiver board's output for HDMI compliance, the data signal is larger than 5 volts. I am using no emphasis or de-emphasis turned on, just the signal as is. Why are the data signals out of 5v range? Are the RJ45 category cables allowed to be outside of the HDMI spec or are all data lines and clock signals required to be with the HDMI specification?
I also would would like to confirm the schematic with the data sheet, since the schematic for the driver board has CS (pin16), SDA(pin17), and SDC(pin18) but the other data sheet with the pin descriptions state pin 16, 17 and 18 are not to be connected. If there is a update schematic, please let me know.