Part Number: TXE8124-Q1
Other Parts Discussed in Thread: TXE8124,
Tool/software:
hi,
A question about TXE8124 latched output.
1. how to understand this sentence "Latched outputs with high-current drive maximum
capability for directly driving LEDs" ?
2. See picture below, TXE8124 is powered by always-on 3.3V power rail , and reset is pulled up by this always-on 3.3V through 10K.
MCU SPI signals connect to TXE8124 , and control P0.0 to HIGH level.
My question: if MCU is power down, but TXE8124 still powered and there is no reset , can P0.0 keep HIGH level ?
thanks!