Part Number: TL16C752C
Tool/software:
Nice to meet you.
I am currently developing using the TL16C752C.
I am developing with the communication settings set to no parity.
Sometimes, when I look at the Line Status Register (LSR), a parity error occurs.
Is it okay to ignore this parity error?
Also, why does a parity error occur with a no parity setting?
The settings are as follows.
Crystal used: 19.6608MHz
Baud rate: 2400bps
Data length: 8 bits
Stop bit: 1
No parity
DLL: 0000 0000
DLH: 0000 0010
FCR: 0000 0111
MCR: 0000 0100
LCR: 0000 0011
Thank you in advance for your help.