This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL16C752C: Parity error with no parity setting

Part Number: TL16C752C

Tool/software:

Nice to meet you.

I am currently developing using the TL16C752C.

I am developing with the communication settings set to no parity.

Sometimes, when I look at the Line Status Register (LSR), a parity error occurs.

Is it okay to ignore this parity error?

Also, why does a parity error occur with a no parity setting?

The settings are as follows.

Crystal used: 19.6608MHz

Baud rate: 2400bps

Data length: 8 bits

Stop bit: 1

No parity

DLL: 0000 0000

DLH: 0000 0010

FCR: 0000 0111

MCR: 0000 0100

LCR: 0000 0011

Thank you in advance for your help.