Part Number: LMH1218EVM
Other Parts Discussed in Thread: USB2ANY, LMH1218
Tool/software:
If only using SMBUS I2C mode in SigCon Architect, will programming still work if I just jumper wire pins 5, 9, 10, and 6 (with J4 7-8 and 9-10 shorted) between the EVM header and the USB2ANY, or do pins 2, 4, 8, and 3 on J3 also need to be connected to the USB2ANY programmer?
I know for SPI mode that Resistors R26-R31 level convert to 2.5V, but is there a reason they are still connected for SMBUS mode as a pull down or are they unused? Similarly, it's not clear if pin 3 is used by the USB2ANY in SMBUS since this is the address bit registered by the LMH1218 device to set the I2C address and set through a resistor.