Part Number: TVS2700
Tool/software:
Hi,
I have a design requirement where I need to survive a IEC 610004-5 pulse with a 1.2/50us surge instead of a 8/20us used like in the data sheet, and the typical test. If I do straight line interpolation between the 8/20us, and the 10/1000us max surge current, it looks like we have some head room. I'm interpolating between the 2 points given by the decay time vs max surge. So the two points are (20us,40A) and (1000us,4A).
My question is: do you think this is a reasonable method to estimate max surge current?