Part Number: DS250DF230
Tool/software:
Hi,
According to the device's datasheet (Section 7.5), the TEMP lock parameter was validated using a temperature ramp rate of 3 °C per minute.
Could you clarify the expected behavior of the device when subjected to a temperature ramp rate exceeding 3 °C per minute (e.g., approximately 10 °C/min)?
Specifically, is there a risk that the device may lose CDR lock under such conditions?
Thanks,
Lior