Part Number: DP83826E
Tool/software:
Hello,
I would appreciate your help regarding the following issue.
We use TI PHY DP83826E in 2 projects:
- First project which is based on Infineon XMC4800 worked so far with TI’s PHY: DP83826E.
- Second project which is based on TI F28P650DK worked so far with TI’s PHY: DP83826E.
In both projects, we recently got new boards with same PHY of type DP83826E, but different date codes.
With the new PHYs, we experience the following issue:
- Port Link acting as active high and not active low (as opposed to our previous boards).
- We cannot establish ETHERCAT connection.
We can't establish a connection with an ECAT master such as Beckhoff controller.
In both projects, the only thing which is changed in the new boards, is the PHY date code.
When we replace the new PHY with old PHY – ECAT communication is ok.
The "old" PHY which is working properly has these details printed on it:
- 826E
TI 198
ALSE G4
The "new" PHY which is not working properly for us:
- 826E
TI 218
A2VN G4
- 826E
TI 168
AEXF G4
I'd appreciate your assistance with this issue.
Are you aware with any functional modification between these PHYs?