Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83826I: DP83826I with J1012

Part Number: DP83826I
Other Parts Discussed in Thread: DP83826EVM

Tool/software:

Can I please get help with following question:

I am working on schematic design with DP83826IRHBR as ethernet PHY. RJ45 connector J1012F21CNL from Pulse Electronics.

J1012 has different transformer topology than DP83826I datasheet figure 8-2, specifically for receiving path. Can this connector be used with DP83826I? J1006 from the same datasheet matches DP83826I datasheet figure 8-2. Both J1006 and J1012 have the same insertion loss, crosstalk and etc specification. If J1012 can be used, how do I connect center taps (pin 2 and 5) of transformer facing PHY?

Thanks,

Tyler