Part Number: TCAN2450-Q1
Tool/software:
I noticed some issues when observing the PWM output and would like to ask for your clarification on the following.
Here are the details of my configuration: the PWM frequency is set to 200Hz, and the PWM width is configured as 10 bits. During testing, I noticed that when the duty cycle is set to 10 (approximately 1%), the connected LED lights up normally, and the oscilloscope shows a valid PWM waveform. However, when the duty cycle is set between 0 and 9, there is no PWM waveform detected on the oscilloscope, and the LED remains off.
Given the above phenomenon, there seems to be an inconsistency with the confirmed minimum output duty cycle of 0.5%. Do I need to configure any additional special registers to achieve the minimum duty cycle output?
if duty cycle is set to 9, that would be approx 350us On time. That seems fairly long as it relates to slew rate.
thanks,
JJ