Part Number: TCAN1145-Q1
Other Parts Discussed in Thread: ISO7741-Q1, UCC33020-Q1, ISO7742-Q1, ISO7741, ISO7041-Q1
Tool/software:
Hi expert,
My customer (CosMX) is looking for a low power Isolated CAN solution, they need to achieve <1mA quiescent current in sleep mode. And the current solution as below show, do you think it is the best solution? And how to realize lower power with this solution (Customer has tested the current quiescent current is 20mA)?
- Current solution: TCAN1145-Q1 + ISO7741-Q1 + ISO7742-Q1 + UCC33020-Q1 (Isolate TXD, RXD, SPI, INH, WAKE. Do we need to isolate all 6 signals?).
Best Regards,
Ryker