Part Number: TCA9548A
Tool/software:
Hi,
In one of our designs, we’re using this component to isolate the I2C paths to our slave ICs. The goal is to prevent a single I2C slave failure from disabling the entire I2C bus.
For example, if one of the slave ICs fails and pulls the SDA line low (e.g., shorted to GND), the entire I2C bus would become non-functional, and communication with all other devices would be lost.
Looking at the functional block diagram of the TCA9548A, it seems that if a slave device connected to an active channel fails in this way, it could also block access to the TCA9548A’s I2C control interface. Is that correct? If so, would the only way to recover the I2C bus be to reset the TCA9548A and disable the faulty channel?
Thanks in advance for your help!