Thank u MAX,But here i am using only serialiser and i wanted to see only the serializer output. using SN65LV1023ADB in this case what should be the connections of SYNC pin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thank u MAX,But here i am using only serialiser and i wanted to see only the serializer output. using SN65LV1023ADB in this case what should be the connections of SYNC pin
Bhagyalakshmi V,
In that case, you should hold SYNC1 and SYNC2 both low. Under these conditions, the serializer will output serial data corresponding to the DIN parallel data inputs. If either SYNC pin is high, the output is forced to be 111111000000 (the synchronization pattern) regardless of the state of the DIN inputs.
Best regards,
Max Robertson