Other Parts Discussed in Thread: LMH1983
Please advise me on how LMH1983 assert/de-assert NOLOCK signal.
Referring the datasheet, LMH1983 decide NOLOCK condition based on two registers,
LOCK_STEP_SIZE (0x2D) & LOCK1_THRESHOLD (0x1C).
LOCK_STEP_SIZE (0x2D) specifies amount of validation permitted on VC_LF pin
LOCK1_THRESHOLD (0x1C) specifies the number of HIN pulse before the device
Assert NOLOCK.
Q1. Please let me know the precise logic of asserting and de-asserting NOLCK.
Does device refers only LOCK_STEP_SIZE when it de-assert NOLOCK
or checks the number of HIN pulse hit in a window as well?
Q2. I suppose that LOCK1_THRESHOLD check the number of HIN pulse in a specified window.
If so, how much the size of the window?
Q3. On page 28 of the LMH1983 data sheet, there is ate following description.
Setting “1”, into the LOCK_STEP_SIZE may make the lock time long.
What do you think?
To minimize the amount of time that it takes to assert lock,
load the LOCK_STEP_SIZE register (register #45, 0x2D )
with a value of 1, and the LOCK_THRESHOLD register (register
#28, 0x1C) with a value of 31. The effect of this can be
seen in the 'Faster Reaction Mode timing diagram shown below