This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDS95: Grounding input data bits

Part Number: SN65LVDS95

Tool/software:

Can we ground any of input data bits out of 7 input data bits for a channel. will there be any advantage if we ground one bit in every channel or 2-channels.

  • Hi Arun,

    For this deivce you can leave unused input pins floating, or you can use external pull-down resistors of ~ 10kOhms. (Also mentioned in this E2E: RE: WEBENCH® Tools/SN65LVDS95: REFERENCE DESIGN )

    There is no particular advantage to not using input pins, and also please make sure that the channel connections and LVDS sequence from the datasheet is followed. You can find on the "Figure 1. 'LVDS95 Load and Shift Sequences" how the bits are serialized over the output.



    Best regards,
    Ikram