Part Number: THVD1500
Other Parts Discussed in Thread: THVD2410
Tool/software:
Setup:
- Max nodes on the bus = 25, all with 1/8th unit load
- Termination will be done at the last node
- All nodes are connected via CAT5 Ethernet cable in a daisy chain fashion with each node imposing a minimal stub to it's transceiver. A+ and B- correctly applied to a twisted pair. Cable has shield, but a ethernet cable that actually connects the shield will probably not be used.
- Max cable run for the full bus for all nodes is <400ft
- A common ground wire will/can be connected between each node via CAT5 cable
- Master/Slave Architecture on the bus
- Master node will be connected to a PC via a USB to RS485 board setup. Since we only need 1 master node, I'd be happy to make the master node fully isolated and the rest not isolated. That would be within budget if it helps.
- Each node is independently powered inside a slot machine type of cabinet. Customer supplied 12V power supply, not something we control.
- Max baud rate is 200kbps. But we can go down to 115,200 or even 19200 if it gets us reliability with no isolation.
- I will be adding bus biasing resistors to the master node to insure fail safe operation if nothing is driving the bus
Why the hesitancy of isolation? The THV1500 can cost $0.31/unit. But an isolated driver can cost 5x that, and does not include the circuitry needed for isolating the power supply. So more $ and more board space. Which is why I would be willing to spend more on the master node, to prevent the device nodes from having to isolate.
From what I have been researching, the fact that each node is independently powered via a customer supplied power supply is the biggest reason we may NEED to go to an isolated solution due to ground loops. Especially if the 12V power supply used is earth referenced.
Any advice, concerns or reassuring comments that a non-isolated solution can be reliable would be appreciated.
Regards,
Matt