Other Parts Discussed in Thread: TUSB2036
When I run the TI USB EEPROM Burner utility on my TUSB3210 design I get a USB Hub Power Exceeded error in windows.
My designed is set to run on bus power however when I load the EEPROM Burner firmware it wants to consume 500mA.
How can I prevent this from happening? Is the bus/self power mode set using pin21 on the TUSB3210? Or is it set in the firmware?
Thanks.