This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUXHS4212: Regarding the CC controller/PD controller used in conjunction with the TMUXHS4212

Part Number: TMUXHS4212
Other Parts Discussed in Thread: TUSB422, TUSB322, TUSB321, TUSB320

Tool/software:

Hi team,

The customer is considering using the TMUXHS4212, and is also evaluating a controller to pair with this MUX.

Ideally, they are looking for a PD controller with PD functionality, but so far they have only found options like the TUSB422.

However, since the TUSB422 communicates via I2C, it cannot be connected directly to the SEL pin of the TMUXHS4212.

Are there any other PD controllers that can be used in this setup?

Also, regarding CC controllers that can be used with the TMUXHS4212, is it correct to assume that the available lineup includes the TUSB320 series, TUSB321 series, and TUSB322 series?

Best regards,

Kyohei