Tool/software:
Hi expert,
Do we have CAN devices which can meet ARINC 825 standard? Customer (Enpower) wants to use CAN devices in eVTOL and it need to meet ARINC 825 standard.
Best Regards,
Ryker
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi expert,
Do we have CAN devices which can meet ARINC 825 standard? Customer (Enpower) wants to use CAN devices in eVTOL and it need to meet ARINC 825 standard.
Best Regards,
Ryker
Hi Ryker,
I will get a response to you by 8/11. Thanks for your patience.
Best,
Ethan
Hi Ryker,
I am not the most familiar with the ARINC 825 standard, and the standard is not publicly made known. But it looks like generally the physical layers between this and the CAN ISO 11898-2 physical layer are the same. TCAN1043A is compliant with ISO 11898-2 so it will likely be compliant with the ARINC physical layer portion. TCAN1043A requires a standalone controller in order to work, and this controller will likely need to be explicitly ARINC certified. ARINC seems to just configure the CAN IDs, resynchronization, and bit timing which are all part of the software layer.
Best,
Ethan