Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LV1023A/SN65LV1224B questions

Other Parts Discussed in Thread: SN65LV1224B, SN65LV1023A

I just got a customer question on the SN65LV1023A/SN65LV1224B 

 

 

1) Data Sheet for SN65LV1023A/SN65LV1224B, Feb. 2009. In this data sheet is the pinout of the deserializer chip missing. 

 

2) Page 10 of the above data sheet:Deserializer Timing Requirements for REFCLK:

We receive data with 310MHz = 620Mbps. What is the frequency for REFCLK? Do we need 63MHz +-100ppm? Or can we use a clock of 63MHz with +-5% (like defined in the National data sheet)?

The device we have to interface uses 310MHz for the chip internal data serializer, which gives us a data rate of 620Mbps. The data stream has 1 stop, 1 start and 10 data bits. And
now I wonder, what frequency REFCLK should get? Please give me detailed information about this input clock signal. I do not understand, why it is needed. The data sheet defines +-100ppm. And I wonder: 100ppm of what?
 

 

3.) It is easy for me to send a constant sync pattern. If i would send $3F (all 10 bits high) as Sync pattern, the receiver would immediately lock after 4 cycles? Is this true?

 According to the datasheet the deserializer needs at least 4 consecutive cycles of data to go into lock. Is there anything else he needs to be aware of?   

4) If the sending device shows some temperature drift, some voltage drift, on the data stream, does the SN65LV1224B follow this drift or what will happen during decoding?

We want to / have to build a robust interface, which, when locked, stays locked for weeks of continuous operation.

  • 1. The SN65LV1224 deserializer pinout is provided at the bottom section of the table on page 6.

    2. Use this simple formula:

    Serial data rate (Mbps) = 12 x REFCLKFrequency (MHz)

    Remember that REFCLK frequency has to be between 10MHz and 66MHz and the allowable variation (offset) should be within +/-100ppm

    3. That's incorrect. Please see the description of the SYNC pattern on page 3 of the datasheet under the "Rapid Synchronization" section. The sure way of achieving lock on the deserializer is to send the SYNC pattern.

    4. Yes, as long as the incoming serial data rate is within +/-100ppm of the deserializer REFCLK frequency x 12. Outside that tolerance the deserializer will go out of lock and lose byte boundaries.

    Best regards.

    Hassan.