Part Number: SN65LVDT250
Tool/software:
We designed a board that uses the SN65LVDT250 LVDS buffer. Unfortunately the far end receiver mistakenly does not have a termination resistor (missing the 100ohm resistor). What are the implications of not having the termination resistor? I know it will affect signal integrity and this varies based on the interconnect. Will the SN65LVDT250 still function and drive it's output properly? I am assuming the output will be rail to rail instead of 350mV as it should be. Is this correct? I also assume we would need to operate the interface at a much slower speed?