Part Number: THVD1424
Tool/software:
Hello, I'm not finding in the datasheet what is the resistance values of the internal pull-ups and pull-downs on RD, DE, D, TERM_xx, SLR, H/F. What's the minimum resistance value of these pull-ups and pull-downs?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: THVD1424
Tool/software:
Hello, I'm not finding in the datasheet what is the resistance values of the internal pull-ups and pull-downs on RD, DE, D, TERM_xx, SLR, H/F. What's the minimum resistance value of these pull-ups and pull-downs?
Clemens is correct, you can use the input leakage max/min and Vcc to calculate the minimum resistances. I believe the actual design values are around 2M ohms but since these resistors are not laser trimmed, there can be a large tolerance of 30%. There is a bit of margin built into the leakage specs so 1.1M ohm is quite pessimistic and likely larger than that in real life.
-Bobby