Part Number: TL16C752D
Other Parts Discussed in Thread: TL16C754B, TL16C754C
Tool/software:
Hello guys,
One of our customers is using the TL16C752D. When they use the TL16C752D,
they sometimes encounter an phenomenon similar to No.3. problem
("The TL16C752B(54B) can clear the just set THRE interrupt condition
if the IIR read is coincident with the THRE setting.") of the following errata.
TL16C752B Errata
www.ti.com/.../sllz049.pdf
TL16C754B Errata
www.ti.com/.../sllz048.pdf
At this moment, they have the following questions about the TL16C752D.
Could you please give me your reply?
1. Has this TL16C752B/754B errata been fixed in the TL16C752D and TL16C754C?
2. What is the value read from the IIR when the errata phenomenon occurs? Is it IIR[5:0] 0x01?
3. If it is difficult to implement the "Work Around: Read only the IIR that corresponds
to the channel that generated the interrupt", are there any other workarounds?
Your reply would be much appreciated.
Best regards,
Kazuya.