This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB2E221: Orderable devices with QFN package

Part Number: TUSB2E221

Tool/software:

Dear TI support,

I'd like to use TUSB2E221 with QFN package, I can see 2 options on TI web:

TUSB2E2211005VBWR

TUSB2E221I1005VBWR

But it is not clear to me what is difference between these devices, datasheet says 0 to 70 vs –40 to 85 in datasheet (table 4-1) but also datasheet says -40 to 85 for both in the Package option addendum, and TI web says -40 to 85 for both. Is operating temperature really the same for both devices? If yes then I can use any of them since they are equal, right?

Thanks!

Best regards

Libor