Other Parts Discussed in Thread: ESD2CAN24-Q1, SN65HVD234, ESDS452
Tool/software:
The maximum voltage rating of the device is plus/minus 16V, thus I find the "usual" ESD TVS choices of eg. NUP2105 or ESD2CAN24-Q1 not suitable due to their high clamping voltage above 16V.
I've chosen a TVS: ESDS452DBZRQ1, which clamps betwee 7V and 14V which I find much more sufficient.
However, in the field we're experiencing many faults, and it's always the TVS which has been damaged and typical shows 0-2ohms on one or the twpo TVS' in the device.
Was it a bad choice? Is the NUP2105 or ESD2CAN24-Q1 really suitable for protecting the transceiver? And if so; why? (When the clamping specifications is above the trasceivers maximum)
Now I'm considering changing the trasceiver to the SN65HVD234, which features a plus/minus 36V specification, thus the NUP2105 or ESD2CAN24-Q1 would be sufficient.