Tool/software:
The datasheet says the output pins are with internal pulldown. What's the value for the pulldown? What's the status of the output pins if there is no input or PDB set low? If we connect corresponding pins of two UB926's output together, and when one is functioning correctly, the other one is without input or in power down state, will the downstream IC get correct signals?