This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD231: UL certification

Part Number: SN65HVD231

Tool/software:

Our client requires UL certification of SN65HVD231,Could you kindly help supply?

  • Hi Hui,

    One of our engineers is assigned to this post and will get back to you by the end of the week.

    -Bobby

  • Hui,

    This is an older device that did not have plans to get SAE J2962 certification when it was developed, and there are no plans to get it certified now. Have you looked at our newer 3.3V CAN transceivers, the TCAN34xx-Q1 family of devices, to see if they will work for this application? These have gone through official, Automotive EMC testing and may meet the customer's needs if EMC is required.

    Regards,

    Eric Hackett