Part Number: DS90UB971-Q1
Tool/software:
Hello,
I'm looking for a pair of camera serializers and deserializers for 4M 60fps transmission.
Can you recommend a pair that meets my specifications?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB971-Q1
Tool/software:
Hello,
I'm looking for a pair of camera serializers and deserializers for 4M 60fps transmission.
Can you recommend a pair that meets my specifications?
Hi Myungjin,
Could you share the specific resolution which you're using here along with the CSI-2 data type? It's likely that the DS90UB971 would be a good fit here with a MIPI CSI RX rate up to 1500Mbps/lane over a 4 lane interface. This would be paired with a FPD-Link IV deserializer such as the UB9702 or UB9724.
Is there a specific project that this would be for? We'd be happy to help put together block diagrams for a SER/DES solution to meet the system needs here.
Best,
Thomas
Hi Thomas,
Thank for your comment.
The target image sensor outputs 2688(H) x 1520(V) 10bit 60fps with MIPI 4lane.
This is a CAR DVR project that receives QHD camera video in SERDES format.
Can you recommend the best solution for my project?
Hi Myungjin,
Thank you for providing these details. May I know if the data type here is YUV422 10 bit (20 bit per pixel) or RAW10 format (10 bit per pixel)? In both cases the Ub971 would likely be the best fit here. Are there other cameras which will also need ser/des links for this platform?
Best,
Thomas
Hi Thomas,
Data type is RAW10.
I'm thinking about getting a 4K camera later, but for now, only this camera spec. is required.
Thanks.