Part Number: TRS3222E
Tool/software:
On the currently available TRS3222E datasheet - SLLS793A – JUNE 2007 – REVISED AUGUST 2021, there is a footnote to the 6.3 ESD Ratings - IEC Specifications which seems to say that a 1 uF or larger capacitor is required to be used as the bypass capacitor in order to meet the datasheet specifications when only a 0.1 uF is shown as being utilized in the typical application diagram in section 9.2. Is this a typo on the datasheet? Or is it truly a 1 uF bypass capacitor that is required?