This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLIN2029A-Q1: differences to TLIN2029-Q1

Part Number: TLIN2029A-Q1
Other Parts Discussed in Thread: TLIN2029-Q1,

Tool/software:

what are the differences between TLIN2029-Q1 and 2029A-Q1? 

customer feedback: 

With regards to TLIN2029A as an alternative, we see some differences with the original as below. Is this correct?

EMC optimizations (e.g., lopes)

TLIN2029 is optimized for reduced EMC emissions → potentially measurable difference with long cables.

Air-gap ESD (IEC 62228-3)

TLIN2029: ±25 kV, TLIN1029A: not specified → may be relevant for automotive EMC compliance testing.

TI diagnostic features

TLIN2029 offers "deterministic behavior" during LIN faults – mostly irrelevant in standard applications

on behalf of my customer

Thanks and bye
Hanno