Part Number: TPD4E1U06
Tool/software:
Hi Experts,
I am currently using TPD4E1U6 as ESD protection for the MDI Interface of the Ethernet Connection.
Looking at the part this seems to be symmetric. However there are some Pin names Added to the Part.
Can I use the part with the Following setup:
TD- : Connected to Pin6
TD+: Connected to Pin4
RD+: Connected to Pin 3
RD-: Connected to Pin 1
GND: Pin2
NC: Pin 5
Regards,
Alex