Tool/software:
Hello All,
We have implemented the TCAN sleep mode strategy in the following sequence.
1. MCU is powered up with through VCC1 of TCAN. In sleep mode VCC1 and VCC2 will be OFF. So MCU will be OFF.
2. Once any wakeup event gets generated TCAN will transition from Sleep>Restart>Standby>Normal. Once TCAN transitions to Standby Mode VCC1 will ramp up and Power the MCU. We can identify which wakeup event (either from Wake1, 2... or CAN wakeup) occurred, either through SPI interface or CAN interface.
Parker, please let me know if this strategy is correct.
And I have one more doubt like, once the TCAN transitions to Normal mode, can we use Wakeup pins as normal Digital input pins for other purposes?
And Watchdog is SPI based?
Expecting for the feedback on the same!!
Thanks, and Regards
Nishant