This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IR: Inquiry regarding Strap Pin settings for the DP83867IRPAP.

Part Number: DP83867IR

Tool/software:

Hi~

I would like to inquire about the Strap Pin settings for the DP83867IRPAP part, based on the following configurations.

- GMII, 1Gbps, Full-Duplex

4-Level Strap Configuration
PIN NAME DEFAULT SRAP FUNCTION
FUNC FUNC MODE VALUE R-PU R-PD
RX_D0 b00 PHY_ADD1 PHY_ADD0   b00    
RX_D2 b00 PHY_ADD3 PHY_ADD2   b00    
RX_D4 b00 ANEG_SEL1 PHY_ADD4   b10    
RX_D5 b00 Force MDI/X Half-Duplex Enable   b01    
RX_D6 b00 RGMII Disable AMDIX Disable   b0x    
RX_D7 b00 Speed Optimization Enable Clock Out Disable   b00    
RX_DV/RX_CTRL b0 - Autoneg Disable   b0    
CRS b0 - Fast Link Drop(FLD)   b0    
LED_1 b0 - ANEG_SEL0   b0    
LED_0 b0 - Mirror Enable   b0    

Thank you.