Part Number: THVD1426
Tool/software:
Hello:
I am using THVD1426DR in one application set up in auto-direction control at 3MBaud. I wanted to test this circuit with the direction being controlled instead by an IC (as an option on our PCB).
I followed the diagram on Figure 9-5, which alludes to connecting the MCU DIR pin to both RE' and SHDN' (similar to other RS485 ICs that have RE' and DE). However reception does not work on this configuration as the SHDN' pin following DIR would be low. Transmission works. My question is, if I wanted to have the option of MCU control while using this IC, would I need to instead connect RE' to the DIR pin of the MCU and have SHDN' always high?
Thank you.