This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS280DF810EVM: Test PRBS Generator and Checker on TX and RX

Part Number: DS280DF810EVM

Tool/software:

Hi, I have a DS280DF810EVM board and installed Sigcon software. I jumper connected TXP0 to RXP1, RXN0 to RXN1 using the recommended Huber Suhner cables and SMAs, I set channel 0 to enable PRBS generator, and set channel 1 to PRBS checker, but I dont see any signal or CDR lock indicated on the software. 

The settings are all default setting, low level page on the Sigcon all default values; hardware jumpers are set as in the "DS280DF810EVM User’s Guide". 

But I am not getting any signal received or CDR locked at channel 1. Is there anything I am missing to set or config?