Part Number: TCAN4550
Tool/software:
Hello Interface team, I have a customer with an issue regarding TCAN4550. I will include them in the thread.
They are trying to communicate to a car via OBD II ports. They are using the TCAN4550 and it is working well in most cases.I will paste a segment of their email:
"Our current design uses TI's TCAN4550 transceiver. In general, OBD communication works as expected: our firmware can read PIDs successfully from the OBD ports of many test vehicles that we tried. However, we seem to run into issues with vehicles from the Honda brand, meaning both Honda and Acura cars. Firmware sends the OBD request at the standard OBD CAN ID, but never receives any response from the expected CAN IDs. Using a CAN analyzer, I can see a lot of CAN traffic, but none of them are OBD messages. A commercial OBD reader seems to work fine, it doesn't like the car has a problem.
I doubt it is a TCAN issue, but I just wonder if you know of any problems with using TCAN to communicate with OBD port from the Honda brand?"
Thanks!