Tool/software:
Hi
In my customer's appliaiton DS90UB964 are receiving 4 1280 x 720 camera FPD-Link.
All 4 camera data onto CSI-2 Port0 with virtual channels (VC-ID), and same frame size (1280 x 720).
The notice that when doing vibraion test that cause one FPD-LINK channel not stable. it will cause buffer_error happen in that problem channel
however when one port got buffer_error, the will see the other 3 port drop frame, is this correct the DS90UB964 behavior ?