This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA6418E: Does /INT signal trigger in standby mode(Fscl = 0)?

Part Number: TCA6418E
Other Parts Discussed in Thread: TCA8418E, TCAL6416, TCAL9539

Tool/software:

Hi everyone,

Regarding TCA6418E:

1 - I would like to ensure that if any of the input changes while the device in standby mode, /INT will trigger?

In other words if FSCL(which is the same is I2C clock) is 0Hz, is the /INT signal affected?

2 - also is there a similar device that will latch the input so that /INT will only reset upon register read?

  • Hi Marwan,

    I recommend using TCA8418E, as this device has same functionality of TCA6418E, but it also has 10-byte FIFO for remember key-event presses. TCA6418E can only process one event at a time. 

    Regarding TCA6418E:

    1 - I would like to ensure that if any of the input changes while the device in standby mode, /INT will trigger?

    In other words if FSCL(which is the same is I2C clock) is 0Hz, is the /INT signal affected?

    This is dependent on if  the GPIO direction is configured to INPUT through the GPIO_DIR# register (0 = input). 

    The interrupt needs to be enabled for the GPIO too through the GPIO_INT_EN register. If this bit is not set, then a state change on the input pin will not trigger an interrupt on /INT. 

    2 - also is there a similar device that will latch the input so that /INT will only reset upon register read?

    So most IO expanders will release the interrupt on /INT if an input goes back to its original state. For example, input changes state from high to low - this event triggers an interrupt. IF the input goes from low back to high, then the interrupt will de-assert. 

    TCAL IO expanders can latch the interrupt so that only a register read clears the interrupt. Devices such as TCAL6416 / TCAL9539 have the capability to keep /INT = LOW until the input port register is read regardless if the input goes back to its original state. This functionality is configured through the interrupt latch register 0 / 1. 

    Regards,

    Tyler

  • Thanks for your recommendations,

    Also I would like to ensure that if a pin is configured as interrupt source, is /INT  triggered even if the device is in standby mode?

    Kind regards,

    Marwan

  • Hi Marwan,

    /INT is only triggered if there is a state change on the input pin. I assume standby mode, there is no I2C running on the bus, and there is nothing happening on the IO side that could trigger an interrupt. 

    So in standby mode, there is no way for an interrupt to occur. 

    Regards,

    Tyler