Part Number: TUSB211A
Tool/software:
HI ,Please help to check the schematic ,if need to modify , RSTN no need external pull high, right ?
and layout , need PIN2 to short to PIN7 PIN1 to short to PIN8 ,right?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Yes, RSTN does not need to be pulled high, it can be connected to ground with a 100nF capacitor.
layout , need PIN2 to short to PIN7 PIN1 to short to PIN8 ,right?
Yes, correct. Beneath the TUSB211A, the DP/DM lanes should be shorted across these pins, as the TUSB211A does not actually carry the signal through the device.
Otherwise, schematic looks good.
Thanks,
Ryan