Part Number: TUSB1004
Tool/software:
When using the TSUB1004 in PCIe mode,
Is it sufficient to simply set bit 2 (PCIE_EN) of the USB_MODE Register (Offset = Dh) to 1?
Or do I need to set bit 2 (PCIE_EN) = 1 and bit 0 (USB_MODE) = 1?
When using the PCIe setting with Fixed EQ with Linear Redriver Mode, is the following setting sufficient?
// (address, data)
(0x0D, 0x06), // PCIE enable.
(0x0A, 0x11), // Linear redriver, EQ_OVERRIDE and USB 3.2 <= Should CTLSEL be 1h or 3h?
(0x1C, 0x80), // Disable AEQ enable.
(0x32, 0xC0), // VOD control
(0x20, 0x44), // USB connector CRx1/CRx2 EQ setting
(0x21, 0x55), // SSTX1 and SSTX2 receiver EQ